Other Parts Discussed in Thread: DAC61416
Hi i am trying to interface between teensy and dac81416. my spi code:
_spi_settings = SPISettings(spi_clock_hz, MSBFIRST, SPI_MODE0);
pinMode(cs_pin, OUTPUT);
//digitalWrite(_rst_pin, HIGH);
_spi->begin();
}
inline void DAC61416::cs_on() {
digitalWrite(cs_pin, LOW);
}
inline void DAC61416::cs_off() {
digitalWrite(cs_pin, HIGH);
}
int DAC61416::init() {
// soft-reset , por is initiated
write_reg(R_TRIGGER, (0x001A));
// set SPICONFIG: DEV_PWDN=0, FSDO=1
uint16_t def = TEMPALM_EN(1) | DACBUSY_EN(0) | CRCALM_EN(1) | DEV_PWDWN(0) | CRC_EN(0) | SDO_EN(1) | FSDO(1) | (0x2 << 6);
write_reg(R_SPICONFIG, def);
// write_reg(R_SPICONFIG, 0x0A84);
// reading SPICONFIG back
return (read_reg(R_SPICONFIG) == def ? 0 : -1);
}
void DAC61416::write_reg(uint8_t reg, uint16_t wdata) {
uint8_t lsb = ((uint16_t)wdata >> 0) & 0xFF;
uint8_t msb = ((uint16_t)wdata >> 8) & 0xFF;
_spi->beginTransaction(_spi_settings);
cs_on();
delayMicroseconds(1);
_spi->transfer(reg);
_spi->transfer(msb);
_spi->transfer(lsb);
tcsh_delay();
cs_off();
_spi->endTransaction();
}
//the steps necessary to write to the DAC:
//written a dac_write function that uses 3 8-bit SPI writes to write the 8-bit address,
//and splits the 16-bit data into a 8-bit msb and 8-bit lsb.
uint16_t DAC61416::read_reg(uint8_t reg) {
uint8_t buf[3]; // 15-0
_spi->beginTransaction(_spi_settings);
cs_on();
_spi->transfer( (RREG | reg) );
_spi->transfer(0xff);
_spi->transfer(0xff);
tcsh_delay();
cs_off();
cs_on();
buf[0] = _spi->transfer(0x00);
buf[1] = _spi->transfer(0x00);
buf[2] = _spi->transfer(0x00);
tcsh_delay();
cs_off();
_spi->endTransaction();
// check buf[0]
uint16_t res = ((buf[1] << 8) | buf[2]);
return (res);
}
i am trying to give SCLK three 8 bits as its 24 bit frame, is this correct ?
and also the CS is not at all going low. but i have coded right.(figure 1)
Is this something that has to do with the spi clock hertz ? because when i change it i can see spikes in the chip select pin(figure2)
can you please tell me how much hertz should i give to it ?