I'm using an ADS1115 in differential mode with a step down setup of 330K/3.3K Ohm resistors to measure the voltage of a supercapacitor. The range of the super capacitor is 0-360V, with the step down adjusting that to 0-3.6V. I have attached a schematic of the circuit below, but there are two issues with the voltage measurements. The raw voltage being read is negative, and the corrected voltage (multiplying the ads differential input by a constant) starts to show significant inaccuracies (>1V) at high voltages (>100V). Is there an issue with how the input pins are tied to ground? The green wire at the bottom at the - terminal of the breadboard is connected to ground of a separate power supply. The 6.0F capacitor is what's voltage is being measured.