Hello,
DVDD can support 1.65V~5.5V on the datasheet. But all the timing requirements are specified with DVDD@2.35V~5.5V. I don’t see any timing requirements when DVDD<2.35V. Does TI have different numbers from 1.65V~2.35V?
-Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
DVDD can support 1.65V~5.5V on the datasheet. But all the timing requirements are specified with DVDD@2.35V~5.5V. I don’t see any timing requirements when DVDD<2.35V. Does TI have different numbers from 1.65V~2.35V?
-Jason
Hi Jason,
Let me check with the design / systems team whether any of these timing specifications would be affected by DVDD < 2.35 V. For the moment, I only see that SCLK must be limited to 20 MHz or less when DVDD < 2.35 V.
Regards,
Ryan
Any feedback on this request?
Hi Jason,
It looks like the main difference is with respect to the digital input high and low levels. For DVDD < 2.3 V, the input signal must be closer to DVDD or DGND to be recognized as a digital high or low, respectively.
Regards,
Ryan