This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1000-Q1: ADS1000-Q1 Maximum VIN+ and VIN- Relative to GND

Part Number: ADS1000-Q1

Looking at DS REV B OCT2015, just want confirm if the absolute maximum rating on item "Voltage to GND, VIN+, VIN-" is VDD+0.3 instead of just "0.3"

  • Hello, 

    Thank you for bringing this to our attention. You are correct that the Max Abs should be listed up to VDD+0.3, and not to 0.3V

    If the recommended operating  conditions, which are listed correctly, are followed, then all requirements will be met. 

    Regards

    Cynthia