Part Number: ADS4125
Other Parts Discussed in Thread: CDCE72010, ADS4129
Hi,
I need to set up an environment to measure CVBS/COMET signals using ADS41xx/58B18EVM.
For EVM ADS4125's CLKP/M,
- Select option 2
- Install FLT1 and VCXO1

For EVM ADS4125's INP/M,
- CVBS/COMET Tx chip
There are some questions,
- How can I sync them and be in phase if use the CVBS/COMET Tx chip instead of the red box below?
- What is the LVDS data rate when running at the maximum ADC sample rate (125 MSPS)?
- Can the LVDS data lanes be configured as 2-lanes or 4-lanes? Or is it just fixed 6-lanes?

Thanks a lot!
Best Regards,
Mike