This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DELTASIGMAEVAL-GUI: ADC Evaluation Software Collecting Data

Part Number: DELTASIGMAEVAL-GUI
Other Parts Discussed in Thread: ADS114S08EVM

Hello,

I am working with the ADS114S08EVM and I want to collect the Data with the Delta-Sigma ADC EvaluaTIon Software.

The Software recognizes the correct Evaluation board, the Registers are set correctly and the 4-wire RTD Sensor is connected to the correct inputs.

But the Data Analysis client displays nothing. What could be the problem?

Regards,

Lukas

  • Hi Lukas,

    Welcome to the E2E forum!  First of all, did you press the Collect Data button?  Also note that the number of samples selected is 2048 and the default data output rate is 20sps, so for this many samples to be collected you need to wait 102 seconds until all of the samples are collected before you will see anything on the display.  If you keep pressing buttons during the data collection phase, the GUI will stop working and the EVM and GUI will need to be restarted.

    When the Collect Data button is pressed, if data is in the process of being collected you should see one of the LEDs on the EVM flash on/off about once a second.  

    Best regards,

    Bob B