Other Parts Discussed in Thread: ADS127L11
Hello,
My customer needs the following specifications as mandatory ones and I think ADS131M02 is the best fit device, but it has 2 channels. Can it be used as a single-end input single channel ADC by configuring like AIN0N=GND and 3h[9:8]=01 to have input signal only at AIN0P? Or do you have another proposal other than ADS131M02?
- Single-end input
- Resolution of 20bit or more
- SPI interface
- Fs>=20kHz
Best Regards,
Yoshikazu Kawasaki