This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102EVM: ADC128S102EVM Power Supply

Part Number: ADC128S102EVM

I need to interface to the ADC128S102EVM board through the J26 SPI port

Can I use the Precision Host Interface board as just a power supply and voltage reference?

Can I just plug in the USB but not connect using the Control GUI software. 

Will/are it's SPI bus lines from the PHI going to interfere with extern SPI on J26? 

I was hoping that if the Control GUI software was not running/connected, the SPI outputs from PHI are disabled/tri-stated.

Thanks