Hello team,
I received a question from the customer.
Is it ok to apply such voltage waveforms to AVDD and DVDD?
Applying a power supply with a rising waveform like this often results in no output when CONVST is input to the ADC.
Yellow is AVDD (5V) and green is DVDD (3.3V).
Both are 1.0V/div, 500us/div.

I asked this question because I could not find the sequence of AVDD and DVDD input even after reading the Power Supply Recommendations in Chapter 9. If the customer applies a linearly rising power supply, the system operates fine.
Regards,
Masa