This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-ADS1219: Simultaneous data acquisition from two BOOSTXL-ADS1219 EVM + MSP-EXP432E401Y launchpad

Part Number: BOOSTXL-ADS1219
Other Parts Discussed in Thread: MSP-EXP432E401Y, SYSCONFIG, ADS1219, ADS122C04

Is there an easy way to extend the capability of the BOSTXL-ADS1219 and MSP-EXP432E401Y launchpad combo to support support data acquisition from two BOOSTXL-ADS1219? I would like to modify the I2C device address on one of the boostxl boards from the default and either stack them on the same bottom launchpad slot or plug the two boards separately in the top and bottom launchpad slots. I think I would also need to modify the GUI to add the option to pick the device I2C address from which data needs to be acquired. Is the source code for the GUI available for modification?