This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8860: ADS8860 data retrieval and interpretation

Part Number: ADS8860


I have two questions regarding to 8860 reading

1. According to data sheet, it is a 16-bit ADC. But nowhere can I find info on how to convert 2 bytes to voltage. The following is how I do conversion:

	adc_8860_val = a_SPI1_3_RxBuf[0] * 256 + a_SPI1_3_RxBuf[1];
	adc_8860_val = adc_8860_val * 3.3f / 65536.0f;
Is it the correct way?

2. I use 3-wire CS mode without busy indicator. From CS high to CS low, I delay 1ms, which is very long. However, according to data sheet, as long as it's longer than max-conversion time, it should be OK. Am I right?