Hello,
In section 10.1.2.1 of the latest (Revised Jan 2017) ADS1299 datasheet, the dc lead off example suggests setting LOFF register to 0x13
This contradicts the register description which says that
Bit 4: is reserved and should be always 0
FLEAD_OFF[1:0]: These bits should be 00 for DC lead-off
Is this is a mistake in the datasheet?
If it is, then should the correct value for LOFF be 0x00 for enable DC lead-off detection with lead off current set at 6 nA and comparator threshold set to 95%P and 5%N?
Ankit