Part Number: ADC09QJ800
Hello,
I am looking how to calculate the SYSREF for the case:
800Mhz clock, 9-Bit, 8B/10B, 4 Lanes.
Sincerely,
Giora
-
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC09QJ800
Hello,
I am looking how to calculate the SYSREF for the case:
800Mhz clock, 9-Bit, 8B/10B, 4 Lanes.
Sincerely,
Giora
-
Hi Giora,
Looks like you are looking at JMODE3. In JMODE 3 with 800MHz clock the serdes rate = DEV CLK X R factor from table 8-16 Operating modes. R = 12.5

Serdes Rate = 800MHz x 12.5 = 10Gbps.
Sysref freq = Serdes Rate / (K x F x 10 x n) Where n is positive integer 1,2,3........
From Table above lets pick K = 32, F = 5, n = 1
Sysref Freq = 10Gbps/(32 x 5 x 10 x 1) => 6.25MHz
Regards,
Neeraj
Gill,
thank you.
Giora