This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53002: Is there a DAC chip controlled by PWM input?

Part Number: DAC53002
Other Parts Discussed in Thread: XTR111,

Hi TI

   Is there a DAC chip controlled by PWM input?

  Is there a DAC chip controlled by PWM input? Because the control terminal is FPGA, only two pins can be used, and the external needs to output two channels of 4~20mA signals, so we want to find a DAC chip that can be controlled by PWM, and then use XTR111 to convert the output voltage to 4~20mA.