Other Parts Discussed in Thread: DAC81416
In my project, I want to produce as many analog outputs as possible.
In detail, i'm trying to make the system that can read external code (ex. MATLAB) or saved code and produce analog voltage outputs to each pin according to the code.
ex.
As time steps proceeds,
1 pin : 1V - 2V - 3V - 3V - 1V - ...
2 pin : 2V - 1V - 3V - 1V - 2V - ...
3 pin : 1V - 2V - 1V - 3V - 1V - ...
...
Each pin should be controlled independently, but with every pin time synchronized. I need as many output pins as possible (at least 64, more the better)
From my colleagues, they suggested using many DACs together, but i wonder if those DACs can be controlled all together with time synchronization.
If there are appropriate solutions for this application, I would appreciated it if you could recommend it.
Thank you