Hi Team,
May I ask a question about ADS8661, in the datasheet, sampling frequency is 1.25 MSPS, but input bandwidth is only 15k.
Previously I used another ADC IC which sampling frequency is 500ksps and –3dB Input Linear Bandwidth is 1.6Mhz.
May I ask what's the connection/relationship between sampling frequency and input bandwidth?
And is ADS8661 suitable for DC current signal sensing circuit which bandwidth is 100khz to 1Mhz (PWM controlled circuit)?
Thanks in advance!