Part Number: TSC2004
The TSC2004 touch controller is connected to a four wire resistive touch screen and to a uProcessor via I2C. The product has just enetered production and some units stop behaving correctly, the touch position reported is not correct. When the touch signals are checked with a scope probe some noise can be seen on the signals and usually the action of probing clears the issue temporarily. The filters in the touch controller are on. The problem currently seems to affect about 10% of the units. From the testing we have done it seems to be a hardware issue but so far we have not found what causes it. Once in the 'bad' mode a quick power cycle does not usually resolve the issue. If the unit is powered down for several hours it behaves properly on start-up for some random time period after which the issue starts again. The touch controller an uProcessor are on a SOM with the SOM mounted on a carrier board which has the main power supplies and interface circuitry, the touch screen signals are on a flex cable with the display video signals and are conencted directly to a connector on the SOM, they do not go to the carrier board. Reseating the SOM also clears the issue and seems to resolve it for a long time / permanently. Therre are only a couple of caps and pull-up resistors connected to the touch controller and the touch signals land very close to the controller. Any thoughs on what could casue this behaviour?