Hi Experts,
Good day.
I need your help with the frequency information for SYSREF pins.
Keep safe.
Regards,
Josel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Good day.
I need your help with the frequency information for SYSREF pins.
Hi Josel,
It seems SYSREF section was left out of the datasheet here. This function should be the exact same as in the ADC3444 datasheet. Please refer the customer to section 9.3.2.1 Using the SYSREF Input for more details. The main idea is this SYSREF input will align the internal clock divider (if used). If the clock divider is set to divide-by-1, then SYSREF is not needed.
Regards, Chase
If single shot, it can be any frequency as the reset occurs on a low→high transition. If periodic, the SYSREF frequency MUST be an integer multiple of the divided clock's frequency.
Regards, Chase