Part Number: DAC9881
Hi,
i am using the DAC9881 to generate 0V-10V DC signals.

Attached you can find my schematics.
When sending 0x0570a to the device and activating LDAC (Negative pulse with 10us length), the output changes from 0V to approx 150 mV. (Should be 0.5V?).
If i send 0x03f0a3 to the device, the output voltage does not change. If i send 0x00000, the output changes back to the initial value (approx. 0V).


Also attached are two screenshots from the oszilloscope for both codes != 0.
Do you find any problems in my schematic which could explain this behaviour?
Best regards,
Moritz