Other Parts Discussed in Thread: ADS7066
Hi,
I have a question regarding ADS7066.
I connected the evaluation board of this ADC, when I wanted to have a maximal sample rate of 250ksps, the SCLK couldn't be lower than 60MHz.
I need to isolate my SPI interface with opto isolators, so I have the limitation of 25MHz maximum for the SCLK signal.
my question is, why do I need 240 clock cycles per sample?
can I use a slower SCLK for my application?
where can I see the minimal SCLK for 250KSPS?
thank you very much,
Roee Kimchi