Other Parts Discussed in Thread: AMC3330
Hello,
I want to measure a DC voltage and connect it like the schematic on the datasheet AMC3336-Q1 p.26 (typi. application).
The HGND is in the middle of the resistor divider and INP/ INN inputs are connected upper and below the shunt resistor. But DOUT shows me a duty cycle of 50% at 0V, 90% at 1V and 10% at -1V input voltage (like the ac-measurement connection below => HGND connected to INN).
So if I change the connection with HGND from INN to the middle of the resistor divider, I don´t notice any changes.
Is the only change to get a higher accuracy and linearity, but the measure range is unchanged? I thought I can measure from +1V INP to -1V INN means 2VDC instead of 1VAC (peak), but I think I am wrong?