Will the ADC08DJ3200EVM work with Xilinx VCK190 dev board? If they are compatible, can 6 g samples/sec be achieved?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the ADC08DJ3200EVM work with Xilinx VCK190 dev board? If they are compatible, can 6 g samples/sec be achieved?
Jeff,
You can use the ADC08DJ3200EVM with the VCK190 but you can only use CHA in JMODE6 with a sample rate up to 2.56Gsps and only CHA in JMODE7 with a sample rate up to 3.2Gsps, since ADC output lanes DA4, DB0, DB5 and DB7 are not routed on the VCK190.
Regards,
Jim