Hello,
In the datasheet, Fig. 71, in the 10x mode the rising edge of the ADCLK sometimes occurs when DDR LCLK is low, and sometimes when DDR LCLK is high. Which makes sense due to the 2.5x clock ratios.
The confusing part is in Fig. 73. The location of the rising edge can be controlled to happen when LCLK is low (PHASE_DDR[1:0] = 10) or high (PHASE_DDR[1:0] = 00).
If I set PHASE_DDR[1:0] = 00, how will the timing diagram of ADCLK and LCLK look like?
Thanks!