Hi,
I'm currently involved in the development of a PLC-like system in my company. The task I should perform now is to design an affordable ADC 4 channel board with SW/HW selectable input ranges from 0-2.5, 0-5, 0-10, +-2.5,+-5,+-10 V. (also it should be HW 4-20 ma meassuring capable, but this question seems already solved). SPI communication is also a request.
Looking for an appropriate Multiplexor - PGA - ADC or one-chip solution, I have find ads8509 as a 1 channel simple solution, but also a possible MPC509 - PGA280 - ADS1259 combination.
I'm posting here hoping to find some advices about specially designed ICs or proper combination of different IC's.
Thanks in advance,
Carlos Leyva Guerrero.