Other Parts Discussed in Thread: ADS7128, ADS7952
Dear Team,
Do we have suitable solution can replace MAX1239EEE+ ?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
MAX1239 is a 12b, 12-channel, I2C SAR. We do not have anything directly comparable, but here are a few similar options.
ADS7128; 12b, 8-channel, I2C SAR. Uses the AVDD supply pin as the reference, which can range from 2.35V to 5.5V.
ADS7952; 12b, 12-channel, SPI SAR. Requires an external reference.
Regards,
Keith Nicholas
Precision ADC Applications