Hi team, could you help with this problem. the maximum surge voltage is up to 8000, which means the device can work normally or isn't broken?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team, could you help with this problem. the maximum surge voltage is up to 8000, which means the device can work normally or isn't broken?

Hi Alfie,
That is correct. The device can withstand surge voltages that comply with the waveform as outlined in IEC 60065 up to 8kV peak.
Hi Alex,
I'd like to clarify on what you mean by "withstand"? You mean device is not damaged by this kind of surge test? or device can function well (correct output) during this kind of surge test?
Thanks
Scarlett
Hi Scarlett,
Thank you for confirming. You are correct, the device will not be damaged by the surge test at this voltage magnitude and the device will continue to function after the test.
I used the word "withstand" as the device will "survive" in spite of such a high voltage being applied.