Part Number: DAC81416
Datasheet says the minimum reccomended operating Vcc is 9V, however it also says that the absolute minimum can go lower.
What would happen if I operated this device from +/-6V - what other specifications would be affected?
I see previously when this was asked, you requested the author state the output current and operating temperature. In this case we would be using only 8 outputs and the max current from each would be 1mA. (Sadly the original author never answered back, so the question was closed without answer). This would be operating in an industrial environment - but let me turn the question around and ask - what temperature range would we need to keep to enable running on +/-6V rails.
Andy