This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8320: Overshoot and undershoot tolerance

Part Number: ADS8320

Hello,

I have some oveshoot on the SPI signals going to the device and i was wondering if the overshoot and undershoot pulses were shoot enough that it wouldn't cause reliability issues.

The overshoot goes up to 8V and is above 6V for about 1.65ns as picture below:

The undershoot goes to -1.3V for about 3ns as picture below: