Team,
In the data sheet on page 18, the "Data rate error" is indicated in a diagram:
-Could you please clarify the meaning?
-Is this the error that is caused exclusively in the digital area of the ADC? or is it the sum of all error chains in the complete component?
-How is this error rate obtained? Is it characterized on a given lot of ICs? or is it based IC design parameters or simulation?
-Is the below understanding correct and correspond to our definition of "Data rate error"?
1V analogue voltage at the input results in a digital value at the output at DVDD=3.3V and 50°C, which corresponds to 0.995V?
-Are there other errors on the analogue side added to this error (tolerance of the reference voltage, gain error, etc.)?
-Any documents/app note you could share in order to calculate the overall errors on the measurements?
Thanks in advance,
A.