Hello team,
I received a question from the customer.
In 8.2 Typical Application, a 10kΩ resistor is inserted between VDD and VREF, is there any problem without this resistor? The customer seems to have configured the circuit referring to the Typical Application, but he says that even if 5V is applied to VDD, the voltage at VREF is 4.6V. Is there any possible cause for this?
Regards,
Masa