Hi,
I have an application requirement as follows:
The input signal fed to the DAC is LVCMOS CLK and 12-bit DATA.
The desired output frequency of the analog signal from the DAC is a sine wave with a maximum frequency of 45MHz.
Is DAC902 suitable for this application, or do you have any other recommendations?
Thanks.