Based on this circuit design, 15 prototypes were tested on power and found that the input current of the DVDD was 24mA.
One step of testing revealed that when PIN8 (RESET) is pulled to 0V, the input current of the DVDD is also 24mA. When PIN7 (PWDN) is pulled to 0V, the input current of DVDD is also 24mA.
Sending commands to ADS1235 through the SPI interface did not receive any data, all of which were 0xFF. The SPI timing is shown in the following figure.
1. Could you please help check if this principle is correct? What areas need to be modified if they are incorrect?
2. The input current of DVDD is also 24mA, which should be unreasonable. What may be the reason for this?
3. Is the SPI timing of sending commands to ADS1235 in the following figure correct?