The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278-SP: fast clocking issue

Part Number: ADS1278-SP
Other Parts Discussed in Thread: ADS1278

How can the ADS1278-SP be used in high speed (frame sync) TDM mode at 31.25 MHz if the DOUT1 timing is up to 31 ns?

The SP datasheet lists the SCLK and FSYNC to DOUT1 timing as taking up to 31 ns, tDOPD and tMSBPD respectively? At 31.25 MHz, the period is 32 ns, which would leave only 1 ns for round trip board and FPGA setup time. At the datasheet max of 32.768 MHz, the period is ~30.5 ns, which is less than 31 ns so the datasheet seems incompatible with itself. Or am I missing something?

We’re powering DVDD at 1.8V. The commercial ADS1278 shows the max tDOPD and tMSBPD is 25 ns. That’d leave 6 ns for board + FPGA timing, which is doable. Also, out application won't run the ads1278 over the full temperature range.

Thanks,

Chris