Part Number: ADS127L01
Hi,
the datasheet says that offset- and gain-calibration is possible in the SPI interface mode.
Can I also configure this with SPI, and then switch the ADC to Frame Sync interface mode for the actual sampling?
I'm asking because chapter 8.4.2 of the datasheet says that when a change is sensed on the Hardware Mode Pins after power-up the device automatically resets (and thus would reset the calibration registers?).
In the specific sub-chapter 8.4.2.1 for the interface mode pins this is not repeated, yet it is repeated for the filter selection and OSR selection pins. So I am not sure now.
In our application we need to use 4 of these ADCs in parallel via FSYNC Slave mode (master is also possible but we would prefer slave), but we would also like to use the internal calibration registers if at all possible.
Thanks in advance and best regards,
Hans