This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC63004: design a new board with using a precision DAC (SBAA341A) and Precision, low-side current measurement (sboa169b)

Part Number: DAC63004
Other Parts Discussed in Thread: TPS7A8300, TPS7A90, , DAC63002, INA296A, OPA186, TMUX1113, OPA3S328, TLA2518

good morning,

I need to develop an analogue board that allows me to accurately vary the voltage between 0.8V to 4.2V and make accurate current measurements of 10µA. The range of consumption of my circuits is from 10µA to 10mA and the other from 300mA to 1.5A. I found the following application notes:
Power-supply margining circuit for LDOs using a precision DAC (SBAA341A) and Precision, low-side current measurement (sboa169b).

I need 2 NA channels to drive 2 LDOs, I will take these components: TPS7A90 and tps7a8300.
I found the following reference which seems to me DAC63004 well can you tell me if this DAC seems to be able to fulfill my expectations?

Jonathan Navor is following my case but I don't know how to put it in the discussion?

thank you for help 

Alexandre