Other Parts Discussed in Thread: ADS7954
Hi,
I have connected a separate digital supply and a separate analog supply to DVDD and AVDD respectively. The digital supply is always connected to ADS7945 while the analog supply is normally turned off and only turned on when ADS7945 needs to be operated. Is it safe and permissible to keep 3.3 V connected to DVDD supply of ADS7945 while its AVDD supply is 0 V? Besides, how will it affect the power consumption?
Can the PDEN pin of ADS7945 be tied with its CS pin in case of 16-clock burst mode? Moreover, if PDEN pin is set to logic high, would toggling CS pin after its first rising edge result in exiting the power down mode?
Best,
Adnan