Part Number: DAC81404
Other Parts Discussed in Thread: DAC81408
Dear Technical Support Team,
I'd like understand the difference between error spec.
Q1
Does "offset error" include "Offset error temperature coefficient"?
Also Does "Full-scale error" includes "Full-scale error temperature coefficient and "Gain error" includes "Gain error temperature coefficient" , ?
Q2
For example, consider Gain Error,
When outputting 5V at 25°C and drifting to 30°C (5°C) rise,
Gain error" is not applicable since the temperature range is TA = -40°C to +125°C. Instead, only "Gain error temperature coefficient ±2ppm of FSR/°C" only is applicable .
Is this correct?
Q3
"offset error" and "Offset error temperature coefficient" have following test condition.
Why bipolar range minus?
Why is it bipolar but defined as negative? How should the positive side be considered?
---------
Unipolar ranges, AVSS = 0 V Bipolar ranges, –21.5 V ≤ AVSS < 0 V
---------
Q4
What's the difference between "offset error" "and "Zero-code (negative full scale) error" ?
Q5
Are following figures typical spec?



Best Regards,
ttd