hello,I wrote some code for the new project,the one msp5509 communicate with ads 1298 via spi,I initial the spi model on the 5509,and cs set low,reset set high and delay 1s,
and set low then delay 1s,after that I set high,I set start from low to high.
first of all,I send sdatac to stop the continous model,
I tried to send the loop data to the 1298 through the spi,the signal is right,but when I send the read reg command to the 1298,there is no response from it,
I tried to send the write reg command to initial 1298 first,then I send the rdatac command to try to get the continous data from it ,but also have nothing output.
I don't know why I did the same thing as the ads1298 spec on the 78 page,but I can not receive any data from the 1298,no matter which model or which command I send to it.
please help me ,thanks,My sclk is about 1.048M and the ads clk is 2M,so i think is not need to delay when send the multiple byte command.