The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306M25: The Current sampling is not accurate of AMC1306M25.

Part Number: AMC1306M25

The application scenario is current sampling driven by motor servo,This is the diagram:

 

Encountered two problems:

  1. There are burrs in the current sampled by the software when the motor is idling。

 

  1. The sampling current of software is larger than that of oscilloscope when servo load。

oscilloscope current(max)

The current sampled by the software(max)

error

15.35

16.1196

0.7696

24

25.79136

1.79136

30

32.2392

2.2392

 

二、Actual schematic diagram

The power supply:

 

The current sampling:

 

 

 

三、The current solution

Change the R19 resistor to 1Ω,After modification, the sampling burr disappeared and the sampling was accurate。

This is the graph and the data:

 

 

oscilloscope current(max)

The current sampled by the software(max)

error

16.25

16.1196

-0.1304

25.9

25.79136

-0.10864

32

32.2392

0.2392

Questions:

1.Why does changing the resistance make the current sample correct?

 

  1. Why is R19 resistor still needed for differential sampling?

    If the picture is not clear, You can read the document。

    The current sampling problem.docx