Other Parts Discussed in Thread: DAC8550,
Hi Team, seeking some input
The data sheet says not to drive the V_REF pin internally and externally at the same time indefinitely.
We would like to use an external 3.3V reference instead of the internal 2.5V reference.
I looked around the website, but could not find anything on how much time is available to switch the reference voltage.
Our SPI signals will not be ready to disable the internal reference for ~30ms.
How long can we place an external reference on this pin while the internal reference is enabled?
Also,
We are using a supply VDD of 3.3V, and a VREF of 3.3V from a bandgap.
In our current design, the VREF pin will come up to 3.3V before VDD is at 3.3V.
Is this acceptable, or should we consider changing the design?
What happens to the output voltage while VDD increases to 3.3V and VREF is already set to 3.3V?
_______
Thank you.
-Mark