Hi Ti,
this could be a silly question, but I need to ask: Why is the minimum reference voltage 2.4V?
Even with the highest reslotion of 24 bit, 1 LSB is still only about 0.5µV. It seems to me, that when you use for example a reference of 0.5V, you can use a lower resolution, which means less power usage, which would probably also decrease the noise. Also, when you work differentially, 0.5V is more than enough for EXG applications.
Pieter Willemen
Antwerp, Belgium