Hi TI expert
Could you pls help to explain how to define the formula to measure the voltage input on ADC channel.
Add more information: we want to measure one voltage with upper limit is 3.3V connect with AIN0, then which FSR shall we choose? is +-4.096?
Is the formula correct? voltage = 4.096* adc / (0.193* 4095), 0.193 is the factor of input voltage, 4095 is the Dec value for 12bits.
Thank you!
BR
Weicheng