This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5573: Can I switch the 4 internal DACs independently to High-Z output?

Part Number: DAC5573
Other Parts Discussed in Thread: DAC53004, DAC63004,

Is it possible to switch the PowerDown modes (via PD0, PD1 and PD2 bits) independently per channel on the DAC5573 (or DAC63004/DAC53004)?

As example - Is it possible to get the following output voltages/High-Z's at the same time: Vout A to 2.5 V, Vout B to High-Z, Vout C to 2.5 V and Vout D to High-Z (with Vref = VDD = 5V)?

As I understand the register description in the datasheet on page 16 (DAC5573), this should work.

However, this is not explicitly mentioned in the description of the "Power-Down Modes" on page 23-24 (DAC5573).

 

Same question for DAC63004/DAC53004.