Other Parts Discussed in Thread: REF6041,
Hi,
In the datasheet it is mentioned that when exiting SLEEP mode there is a small current consumption from the VREFP/N inputs. since I am using LM4040-4.1V for the reference with required capacitors, I need to know:
- what is the maximum amount of possible current through this pin to see I can supply it (and for how long does this current exists..)
- In normal operation can I assume load of about 40K so the current is max 4.096V/40K which is less than 1mA...