This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300: AFE4300 ESD support

Part Number: AFE4300
Other Parts Discussed in Thread: TPD1E01B04

Hello TI Team,

I need support about ESD protection for AFE4300. At moment the input stage of measuring pins has additional ESD diode to protect the IC.  During the ESD compliance tests When we applied more than +/-3 KV to the electrode the respective pin of AFE4300 is damaged . The input impedence of AFE4300 PIN becomes too low (100 ohm ) and if I try to take a measure it is completely  wrong. ESD diode after ESD applied is not damaged so I really don't understand what happens.

Probably clamping  or breakdown voltage of ESD diode are too high compared to the tollerance AFE4300 pin but I am not sure about that.

Do you have any advice or suggestion? Should ESD diode have different characteristics than ESD7361HT1G? I choiced it due to low capacitie.

Below you can see the electrical schematic of input stage ( compents and their value) .

• L1 ferrite→ WURTH 742792041
• R1/C1→ 10 KΩ / 4.7μF
• D1 ESD diode → ESD7361HT1G

Thank you in advance.

Regards,

Gaetano