This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3562: Reference design with LVDS output with cable

Part Number: ADC3562
Other Parts Discussed in Thread: ADC3662EVM

Hello team,

My customer is considering to use ADC3562 with LVDS output to FPGA via FFC (Flexible Flat Cable).

Customer is going to use ADC3562 with 10MSPS, so datarate would be 160MHz with single lane, 80MHz with dual lane.

However, the customer has never done such high speed LVDS design with FFC, so they would like to refer to our example design.

On the ADC3662EVM, the LVDS output is connected to Caputure Card via inposer board (PCB).

Is there any reference design of ADC3xxx ouput connection via cables?

If not, is there any reference design (cable connection) with similar LVDS speed?

Best Regards,

Kei Kuwahara