Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8820: Impact of input offset voltage of following op-amp and high slew rate

Part Number: DAC8820
Other Parts Discussed in Thread: OPA227, , OPA827, OPA828

Data sheet recommends using OPA227 with the DAC8820 due to its low input offset voltage (+/-5uV). However, OPA227 slew rate (2.3V/usec) is too slow . I have searched for op-amps to use with the DAC8820 with low input offset voltage AND high slew rate (200V/usec or greater). There is nothing close to the OPA227 +/-5uV spec.

I am looking to output a voltage from the DAC & opamp with 800nsec total delay to settling within 1%, with the output range of 0 to +10v (hence the high slew rate). After the DAC's output settling time, I have approx. 100nsec allocated to the slew rate to get from 0V to 10V (therefore slew rate should be > 100V/usec).

If this op-amp specs combination is not possible, can you please point me to the impact of a high input offset voltage (and other relevant specs of the op-amp input) so that I can determine how these will affect my DAC-to-analog voltage fidelity?

Thanks.