Other Parts Discussed in Thread: ADS1258
Hello,
I have a PCB that I want to use a ADS1258EP on. The sensors I will attach to the inputs will span 0V - 4.096V. I plan on running the device in autoscan mode with the following pin configuration: Vref=4.096, AINCOM=2.048V, AVDD=5V, AVSS=0V, DVDD=3.3V. If I want to maximize the converter span is the correct approach? Or should I use Vref=AINCOM=2.048V. I realize that there will be some unused head space (.06 on each side of span). I did search through the converter forums and there seems to be some confusion about this topic. Thanks for any input
Scott Metzger