This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8568: Offset appear on converted data at low temperature on some channels

Part Number: ADS8568

Hello,

We use the ADS8568 in one of our designs to monitor 60 Hz signal quality.

We have a signal stability problem at low temperature in our qualification tests. 
The problem occurs on at least ONE channel of SOME systems only.  It is very repeatable when a system has the problem.
At around -10 to -20 deg C, we see an offset of some ADC counts (32-64) appear on the data.... 
The duration of the presence of this offset is variable and disappear when the temperature goes back over -10 deg C.
This offset appears instantly, so it's not a question of analog drift.

We have made a subtraction of raw data on channel 1 vs channel 2 to detect this offset....   So, at the same time, problem is present on channel 1 but not on channel 2.
We also have frequency analysis algorithm that detect frequency change (60 Hz) in the application, and it is detected on channel 1.    

Here is a quick description of the conditions:

- 60 Hz signal is generated from a quality voltage source (Omicron);
- The same 60 Hz signal is connected to all the channels;
- All channels have the exact same design (Input stage, low pass filter, ...);
- Sampling Rate is low at 7680 Hz;
- Same signal is used on the 4 CONVST pins;
- Configuration Pins:  RANGE 4x VREF/ EXTERNAL REFERENCE / HARDWARE MODE / PARALLEL

- All capacitors and other components are as requested by the datasheet and the evaluation module.

- All digital interface timings have been checked. 
- We have seen an issue with some BUSY to READ delay on the forum.  We applied a larger delay with no success... (As requested by an updated datasheet)


I went thru all the forum posts about the ADS8568 and the one named "ADS8568: Missing codes when device is cooled" looks a bit similar to our problem,

Can you help us with this problem ?