Other Parts Discussed in Thread: DAC37J84, LMK04806,
Hello,
My customer wants to use the DAC37J84 under the following conditions.
- DACCLK P/N (Input CLK) = 1258.2912Mhz (From LMK04806)
- DACCLK (PLL out) = 943.7184Mhz (DAC PLL used, PLL Lock ok)
- pll_n=4, pll_p=5, pll_m=3, H-Band(pll_vcosel=0), pll_vco=21
- DAC Fs = 943.7184Mhz
- Line Rate = 9437.184Mhz
- JESD Core clock = 235.9296Mhz (LineRate/40)
- FPGA REF CLK = 314.5728Mhz
- Full-Rate, Mpy=10, Serdes Refclk = 235.9296Mhz (div_by_4)
- SYSREF = 3.6864Mhz (9437.184 / (80*32) = DataRate/(N x K))
- LMFS = 8212 / K=32, F=1
Q1) please review whether the following Register values set by the customer are correct for the configuration.
Q2) When the DAC37J84 operates with the above settings, the following error occurs. Please advise on the cause of this issue and how to solve it.
- DAC Sync stays low
- Config100-107 = 0x0008 Lane FIFO errors: bit3 = write_error : Asserted if write request and FIFO is full
Q3) If they set jesdclk_div Setting (Config37) = 0xC000, DAC Sync turns to high, and Lane Alarm (config100~107) is also 0x0000.
If Jesdclk_div is set to 2, 4, 8, or 16, sync is low and Lane Alarm also occurs. Is there a rule to set Jesdclk_div?
Thank you.
JH